Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG TX & RX Buffer size Restriction ?

Posted on February 04, 2016 at 13:55Hi all,           In BlueNRG chat application, i can able to transfer and receive data if  the packet size was 20 or below. When i change the packet size more than 20 bytes , communication doesn't started. But i n...

BlueNRG-MS Max througput

Posted on February 13, 2016 at 09:14Hi,We are using BlueNRG-MS  with Andorid 5.1x. using GATT profile. Need to know what is the max throughput we can achieve here? What seetings are needed to achieve the same? Currently we ae using conection interwa...

rajaram by Associate
  • 869 Views
  • 1 replies
  • 0 kudos

How can i get BlueNRG Firmware version ?

Posted on February 19, 2016 at 14:35Hi all,          I need to know, BlueNRG firmware version which is flashed in my BlueNRG chip without using BlueNRG GUI window. What are the possibilities to get this ?  Can i get this from SPI ? or give me prope...

Migrating BlueNRG from stm32l1xx to stm32f1xx

Posted on March 03, 2016 at 04:23Hi everyone,I'm doing a project to communicate between stm32f107 to blueNRG. I also check the sample controller from STM evaluation board which is based on stm32l1xx. What I found that there are many differences betw...

tnthinh by Associate
  • 736 Views
  • 1 replies
  • 0 kudos

AT+S.SCAN problem

Posted on March 08, 2016 at 15:00Hi, I performed  a session of test with this spwf01 module in station mode with a router wifi.I saw a problem that it accours sometimes during a scanning for  find wifi network.  I sent a command to the module:AT+S.S...

sandro by Associate
  • 806 Views
  • 1 replies
  • 0 kudos

Error : Command not found

Posted on March 03, 2016 at 09:34Hai !I am having two wifi modules and I have configured the initial settings.In both the modules I am getting the status ''Handshake Complete''.After this i tried to give command ''AT'' and both giving the response O...

Nandy K by Associate II
  • 1550 Views
  • 3 replies
  • 0 kudos

STEVAL-SP1ML915

Posted on August 06, 2015 at 00:02Reading and writing the SPIRIT1 radio registers directly, doesn't seem to work.Here is one simple example...AT/SR36=10OKAT/SR36?36=88AT/V reports SP1ML-915 HW:V1 FW:V0.12Is there a more recent firmware version that ...

jeffm by Associate II
  • 1859 Views
  • 3 replies
  • 0 kudos

Ways to send AT Commands

Posted on February 10, 2016 at 16:24Hi,Now I am sending AT Commands  in two ways1. through Tera Term 2. through UART ( Wifi Module Connected to my MCU via UART )Is there any other way to send AT commands ?Is it possible to send AT commands on air ??...

Nandy K by Associate II
  • 2271 Views
  • 3 replies
  • 0 kudos

SP1ML-915 custom firmware

Posted on October 05, 2015 at 02:38I'm wanting to load a custom firmware onto the SP1ML-915, as I'd like to implement abilities I can't get through the existing AT command set. Where can I find documentation about how the STM32L151RB is connected to...

pete2 by Associate
  • 1363 Views
  • 2 replies
  • 0 kudos