Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Spriti1 application

Posted on March 23, 2017 at 17:03Hello everybody,I have the STEVAL-IKR001Vx evaluation kit and the SDK-2.0.1 and SDK-2.2.0. I have been trying to work with the GenericBasic_A and B. Both files compiled without any error in IAR and Keil v4. However, ...

idris by Associate II
  • 626 Views
  • 0 replies
  • 0 kudos

Spirit1

Posted on March 23, 2017 at 16:47Hello everybodI have the STEVAL-IKR002Vx developmental kits and downloaded the SDK 2.0.1 and 2.2.0. I have been working on the SDK_BasicGeneric_A and B. The code compile fine in both IAR and KeilV4. However, nothing ...

idris by Associate II
  • 754 Views
  • 0 replies
  • 0 kudos

SP1ML: RSSI at 1 meter is too low (-90 dBm)

Posted on February 04, 2016 at 23:02I have two SP1ML modules, transmitting 11 dBm. If they are really close (1 cm), the RSSI is around -30 dBm,  when the distance is 1 m, the RSSI goes down to -90 dBm. It seems that these values are too low. Anyone ...

logic output max current for ST3232C

Posted on March 19, 2017 at 00:30I'd drive an opto-isolator's LED directly from the logic output of ST3232CTR (VCC=5V). I'd set current with a serial resistor (Vcc - R - LED - 3232's output.  Output=L to light the LED up). I checked 'DocID7454 Rev 1...

st7580

Posted on March 18, 2017 at 20:32I am beginning to experiment with this part but something has me a bit stumped.The eval board says that the transmit filter is configured for a frequency of 150KHz with a sensitivity around 100KHz.However the receive...

gareth23 by Associate
  • 589 Views
  • 0 replies
  • 0 kudos

Mistake in ST3232 datasheet

Posted on January 24, 2017 at 01:05In the http://www.st.com/content/ccc/resource/technical/document/datasheet/group1/40/2c/7f/62/3a/3f/47/3c/CD00002253/files/CD00002253.pdf/jcr:content/translations/en.CD00002253.pdf, the introduction text says:The d...

how to enable spbtle-rf dc-dc converter?

Posted on March 16, 2017 at 12:39In order to optimize the consumption in my project i would like to enable the dc-dc converter.The datasheet says ' Optimized results are obtained when the embedded high-efficiency DC-DC step-down converter is used.'D...