Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPSGRF-868 module

Posted on June 21, 2018 at 07:53I am using SPSGRF-868 module on a medical device. I am trying to get the connection established between acquisition board(transmitter) with the Main display board (receiver). Both have this module configured in P2P mo...

BlueNRG-MS reconnection issues

Posted on May 27, 2018 at 20:14 Hi, I'm using the BlueNRG-MS as HID peripheral and having trouble with the re-connection process. In order to reconnect with the central, I use directed advertising. The central recognize the slave and I get pa...

yon hona by Associate II
  • 2741 Views
  • 8 replies
  • 0 kudos

ST7590 Usage and Documentation

Posted on June 29, 2016 at 12:27Hello All.I've been looking at using the ST7590 OFDM Power Line communications module in a project. However I've found the information published on STs website to be very lacking in technical details. From what inform...

SPWF04 writing to socket client fails

Posted on June 17, 2018 at 03:24In my application, we are reading large files from an SD card and transferring them over WiFi to an AP. The SPWF04 is connected to an STM32L4 using UART.Data chunks are sent from the MCU to the WiFi module after openi...

How to get the website certificate ?

Posted on June 15, 2018 at 10:01Hii'm using a SPWF04Sa wifi module and i need to connect to a cloud using https (port 443)There is a way to set the cloud's certificate without using AT+S.TLSCERT command ?I mean : I don't want to set it manually if i...

SPSGRF-868 question

Posted on June 11, 2018 at 10:43Hello everyone,for my project I want to use the SPSGRF-868 Module. I want to know if is it possible to use the module as point to multipoint?My goals is to have a Master that transmit data to two Slaves, and that only...