cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04SA: Where is my NTP request response?

Antonio Roman
Associate II
Posted on February 22, 2018 at 22:40

Hi,

I'm working with SPWF04SA using UART in a custom project. I have a issue making calls to NTP server. I've tried with several servers, but the behaviour is the same, I can't get response.

This is what I send and what I receive:

+WIND:1:Poweron:170216-fd39c59-SPWF04S                                          

+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc.  All rights Reserved:SPWF04SA                                                                         

+WIND:0:Console active                                                          

+WIND:3:Watchdog Running:20                                                     

+WIND:32:WiFi Hardware Started                                                  

+WIND:21:WiFi Scanning                                                          

+WIND:35:WiFi Scan Complete:00                                                  

+WIND:19:WiFi Join:BB:AA:EE:AA:50:40                                            

+WIND:25:WiFi Association successful:MyNetwork                               

+WIND:51:WPA Handshake Complete                                                 

+WIND:24:WiFi Up:0:192.168.50.207                                               

AT+S.SOCKON=ntp.inrim.it,123,NULL,u                                             

AT-S.On:193.204.114.105:0                                                       

AT-S.OK                                                                         

AT+S.SOCKW=0,48                                                                 

AT-S.ERROR:60:IP not ready to send                                            

+WIND:24:WiFi Up::fe80:0:0:0:280:e1ff:febd:f6c5                                 

+WIND:84:NTP Server delivery:2018.2.22:4:21.1.53                                

And, It is interesting this line:

AT-S.ERROR:60:IP not ready to send

This apears 40 seconds after calling NTP server.

And, this another line is also interesdtin too:

+WIND:84:NTP Server delivery:2018.2.22:4:21.1.53

Well, as I can see, efectivily, the wifi module can get a NTP update, but, where is the response packet that I requested with the UDP socket connection to port 123?

I was expecting something like:

+WIND:55: ...

What am I doing wrong?

Regards

AR

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0