Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need ST8500 AND STCOMET information

Posted on February 08, 2018 at 14:13I have done some research on G3-PLC based chips available on market and I selected to buy ST chips. So, could you provide some information about development firmware and all other stuff regarding for software deve...

AP_040 by Senior
  • 938 Views
  • 1 replies
  • 0 kudos

BlueNRG-MS GATT write

Posted on October 29, 2015 at 13:26Hi all,I have a BlueNRG-MS-based GATT server with several characteristics, and I'm able to read and write these characteristics from Android. Now I need to implement a GATT client using BlueNRG-MS to access the GAT...

ivan2399 by Associate
  • 1196 Views
  • 2 replies
  • 0 kudos

Issue: USB and STM32 on Windows 10

Posted on July 14, 2018 at 02:19Hello! I'm having problems with using USB comm ports and STM32. I've used CubeMX to configure the USB as a CDC. When I first upload the firmware to the micro it works well on windows 10, but as soon as I reset the boa...

Changing name on the device?

I would like to change the names of my devices (at the device), and it looks like the BTLE spec says that Write access is "Optional" https://bit.ly/2NYnkvoIs it better to do that (and how would you do that, since it's in the aci_gap_init function and...

TJohn.14 by Associate II
  • 749 Views
  • 1 replies
  • 0 kudos