2018-04-03 7:27 AM
hi,
SPWF047Sx, mode AP, FW1.1.0
CA, cert, key loading with AT+STLSCERT + datetime
cert 2x ecc bundle (prime256V1)
client connect to the wifi open.
next is AT+S.HTTPGET=192.168.0.2,conf,45061,2,,,config.txt,
AT-S.Skip CAAT-S.Skip CAAT-S.Loading:1:2AT-S.Loading:2:2AT-S.Loading:3:2AT-S.Http Client Error:2On the client (server https node js), i have bad signature and if i check AN4963 the problem is during decoding the CertificateVerify message:
If the client has sent a digital certificate to the server, the client sends a
CertificateVerify
message signed with the client's private key. By verifying the signature of this message, the server can explicitly verify the ownership of the client digital certificate.
the size of signature sent by server to client (serverKeyexchange) is 71 bytes.
the size of signature sent by client to server (
CertificateVerify) is 70 bytes.
Is it the problem?
(if i use other client (curl) to do same test with same certificate, it works and size of signature for message
CertificateVerify
is 71 bytes)Help!
Thanks
Yoann
2018-04-04 9:50 AM
hi,
you continu investigation but have same problem. we replaced server by openssl (server reference) and the result is the same 'bad signature' during
CertificateVerify
.Signature Algorithm used is:
TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256 .
a help will be appriciate.
thks
Yoann
2018-04-04 12:52 PM
Hello Yoann,
I have just made a connection using a set of keys and certificates generated by me, from SPWF04 to an openssl server. The TLS handshake succeed but the HTTP GET fails because no answer is received to the HTTP request.
The SPWF04 is AP with WPA encryption, the openssl server is forced to use ECDHE-ECDSA-AES128-GCM-SHA256 cipher.
AT+S.HTTPGET=1.112,conf,4433,2,,,config.txt,
AT-S.Loading:1:2 AT-S.Loading:2:2 AT-S.Loading:3:2 AT-S.Http Client Error:4 AT-S.ERROR:111:Request failedI'm attaching the openssl log. Could you please compare the certificate (dumped in the log) with your in order to highlight sensible differences?
Regards,
Elio
________________ Attachments : openssl.log.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxqB&d=%2Fa%2F0X0000000b1F%2FohPmrFpOjVlRa6vE4PJt92E7hf_MvYbojZSphZDuB48&asPdf=false