Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transfer audio files from the phone to a (BLUENRG+STM32+SDcard), without using additional software on the phone?

How to transfer audio files from the phone to a (BLUENRG+STM32+SDcard), without using additional software on the phone? I'm not sure, but I need an FTP profile. I need to realize the transfer of a sound file using the built-in Android / IOS functions...

Upadate BlueNRG firmware using SPI and STM32

Hi,I have a BlueNRG-MS connected through SPI to a STM32L476 like that implemented on ST SensorTile board. The NRG chip wasn't working and I checked that the firmware version is 715. I think 723 is a the latest version and so I am trying to update the...

Resolved! STEVAL-FKI868V1has feature'Automatic acknowledgement, retransmission, and timeout protocol engine'. Does this feature automatic for S2-LP transceiver or it may be enabled/disabled programmatically?

S2-LP transceiver, STEVAL-FKI868V1: it has a feature 'Automatic acknowledgement, retransmission, and timeout protocol engine".1. Does the acknowledgement automatically come from receiver?2. Does this feature automatic for S2-LP transceiver or it may ...

bvn123 by Associate II
  • 1801 Views
  • 3 replies
  • 0 kudos

Resolved! Connecting Bluetooth HID keyboard to STM32

Hi,I'd be grateful for any suggestion what BT module supporting HID I should use to connect BT HID keyboard to the STM32. I see that many popular HC-XX modules support only SPP profile.There are some modules supporting HID profile but all the example...