Is there a programming guide doc for STUSB1702?
For instance, I want to know how to make use of the BMC feature and how to set the voltage levels for power advertisements.
Also, how do I advertise I_BUS > 3A?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-08-30 6:39 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-09-04 3:19 PM
Hi,
The STUSB1702 is a USB-PD controller for Power Source applications (Provider), and with Automotive grade support (AEC-Q100 qualified).
The STUSB1702 is supported with SPC5x family of MCUs, because SPC5 is automotive grade.
https://www.st.com/en/automotive-microcontrollers/spc5-32-bit-automotive-mcus.html
There is no programming guide available. But there are programming examples in the X-CUBE-USB-PD software library.
If you don't need the Automotive grade in your application, it is recommended to use the STUSB1602 instead of STUSB1702.
The STUSB1602 is supported with STM32 Microcontroller family.
The examples for USB-PD Provider are located in the X-CUBE-USB-PD package here:
- STM32CubeExpansion_USBPD_F0_V2.1.0\Projects\STM32F072RB-Nucleo\Applications\USB_PD\MB1303_Provider_RTOS
- STM32CubeExpansion_USBPD_F0_V2.1.0\Projects\STM32F072RB-Nucleo\Applications\USB_PD\MB1303_Provider_PD30