Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wwhen I have the user code in place, if I connect to it or disconnect from it (depending on what user code is in there), it goes into a HardFault exception if the phone touches it.

Environment: Usingng the SPBTLE-1S "postage stamp" on my own board [3v3 supply, external regulator from 12-400V, 100mA available], (using the programming/serial from a STM32F030 Nucleo board) and that works quite well (wish it supported more break...

PGigl by Associate II
  • 554 Views
  • 0 replies
  • 0 kudos

Resolved! Products: Two PCBs Steval-FKI433V2 and S2-LP DK_1.2.1 project example "SDK_Chat.c". How correctly organize echo of Rx data in one of the Steval without connecting it to terminal?

Hello.I use the S2-LP DK_1.2.1 project example "SDK_Chat.c" as the base for two Steval-FKI433V2 PCBs.The 1st Steval with unchanged SDK_Chat.c program is used as a base device, connected to COM-port, the 2nd Steval without connection to COM-port shoul...

bvn123 by Associate II
  • 2528 Views
  • 2 replies
  • 0 kudos

SPBTLE-1S Multi-Channel ADC?

When I read one channel, I get good numbers (using the polled version for now).When I change the MUX after a read to go to the other channel (ADC2, Temperature), I get garbage on all channels.I've read/discarded 12 readings, but even that doesn't eli...

TJohn.14 by Associate II
  • 631 Views
  • 1 replies
  • 0 kudos

Resolved! Kindly give the solution for error: No signature of method: com.crashlytics.tools.gradle.CrashlyticsPlugin.findObfuscationTransformTask() is applicable for argument types: (java.lang.String) values: [ReleaseUnsigned]

I downloaded the latest version available at ST site i.e. Ver 1.07. When I am trying to sync the project the error appears. Same happens with old version also. Kindly help.

NKall.7 by Associate II
  • 1554 Views
  • 2 replies
  • 0 kudos

Resolved! BLE_SensorDemo from Blue Tile DK source file issues.

Compiling the BLE_SensorDemo sources in True Studio does not generate the same .hex as the precompiled .hex provided in the "Firmware" directory. The precompiled .hex works with the BLE Sensor app when loaded onto the BlueTile, but the .hex compiled ...

BPaik by Senior
  • 921 Views
  • 1 replies
  • 0 kudos

Resetting Embedded ST-LINK Debugger on STM32F411RE

Hi, i have a problem and don't find any solution yet. ​I do some mistake and st-link part of my board doesn't communicate to mcu part. ​Actually I'm not sure the problem but, when I search all internet and assume that the problems is this. ​When I co...

Oladi by Associate II
  • 1432 Views
  • 3 replies
  • 0 kudos