Is there a fast method to add Wi-Fi to my STM32F746-DISCO ?
I am developping an application to control an audio system with this evaluation module but I would like to add a Wi-Fi module.
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
I am developping an application to control an audio system with this evaluation module but I would like to add a Wi-Fi module.
Hello, we are developing a device with SPBTLE-1S starting from BLE_Security peripheral example. We choose bond initialization with fixed pin.Everything is working, except the fact that we cannot bond more than 4 devices (smartphones android or apple)...
When I try to do then I get fatal error !git clone --recurse-submodules https://github.com/STMicroelectronics/STBlueMS_AndroidCloning into 'STBlueMS_Android'...remote: Enumerating objects: 83, done.remote: Counting objects: 100% (83/83), done.remote:...
We are working on USB OTG FS using stm32H7 customized controller .It is working fine upto 300MHz system clock and unable to create file above 300MHz clock.Is that something I'm missing out in the configuration?
My PC's OS is Windows 7 64-bit. I had a board IDB011V1. My IDE is IAR 8.40.1. I have installed BlueNRG-LP DK 1.0.0 and BlueNRG-LP Profiles_Lib 1.0.0. Now, I want to build BlueNRG-LP Profiles_Lib 1.0.0 and debug it. But I can not install the driver of...
I have designed a signal source using StuW81300, I want to know when the registers in the chip were set, will the information be lost after power off, and whether it is necessary to reset the register after power on again
Hi all, I am using X-NUCLEO-BNRG2A1 + NUCLEO-L476RG as for preliminary test. I've tested the SampleApp example and it works fine. The final goal is to use the BlueNRG-M2SA in a stm32h753XI custom board + custom antenna. I've tried to generate the Sam...
Hi, I use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .My goal is to describe a card reader (USB CCID class) with the HID service. I tested my HID service with the report map of a mouse and it works I can make it move.Now I send the USB descriptors of th...
My OS is Windows 7 64-bit. I had a Jlink-V9. Now, I want to connect it with EWARM(IAR 8.40) and MDK-ARM (Keil C V5.25). But I cannot connect them. Does anyone know how to do it? Or, does anyone has the document about connecting BlueNRG-LP with EWARM(...