Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! flash example code with Low Layer Drivers ?

Hello,I can't find any example code of flash write or read using LL_drivers, only HAL drivers. I work with Blue NRG and I do have rf_drivers_ll_flash.c with functions that looks like those in rf_drivers_hal_flash.c. But I can't make flash working wit...

Ben1 by Associate III
  • 7957 Views
  • 4 replies
  • 0 kudos

S2LP and CubeIDE, anyone?

I bet mostly everyone who's had their hands on a Nucleo board and an S2LP addon board encountered the lack of support for the CubeIDE integration.So my question is: did anyone get the S2LP-DK or S2LP-SigFox-DK demo projects working with CubeIDE or do...

What is "LOCK_ST" S2LP status 0x14 ?

Hello,I have two custom boards with S2LP cut 3.0, with the same program, but one S2LP can't go in Rx or Tx mode. I tried S2LPPacketHandlerSetTxMode( PN9_TX_MODE ); S2LPCmdStrobeTx(); while(1);I checked the S2LP status ( MC_STATE ), its READY before a...

AndyR1 by Senior
  • 1346 Views
  • 1 replies
  • 1 kudos

S2-LP basic settings and transmitting process.

Hi, I have two S2- LP modul ( Radiocontrolli ) and I would like to test these but I can't start the communication. I use Microchip microcontrollers, the SPI communication is working, TX command OK, I get the nIRQ on GPIO1 ( TX data sent ) , and get ...

LBalo.1 by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

Does BLUENRG-M2SP support Observation Role?

I am currently using BLUENRG-M2SP Nucleo expansion board and STM32L476 Nucleo board. When I execute the aci_gap_start_observation_proc function, I get a 0x46 (BLE_STATUS_NOT_ALLOWED) error.Do I need to make any special settings when executing the fun...

Toro1 by Associate
  • 775 Views
  • 0 replies
  • 0 kudos

L9338 Quiescent current

Dear Sir,I kindly ask you what is the quiescent current value of the driver with EN=HIGH (chip enable) and Vs up to 24V; into the datasheet at page 8/14 is written 2mA max @ Vs<=14V, what should be the maximum value with Vs equal 24V?On page 10/14 is...

FF1 by Associate III
  • 794 Views
  • 0 replies
  • 0 kudos