STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

ST-Link API in C/C++

Hi everyone,  My program isn't establishing a connection to the controller. FlashLoder and Data_Base are located right next to the .exe file in the /x64/Debug folder.  I've attached my program; maybe someone can point out where I'm going wrong.  It w...

STM32Cube Programmer v2.22 SWV not working

Just posting this incase it helps someone with this problem that I encountered recently.I just update to new windows 11 laptop so I started going through the laborious process of installing all my tools including the latest STM32Cube programmer v2.22...

Programmer not able to find target

Hello everyone,I'm using STM32CubeIDE 2.1.0 and STM32CubeProgrammer on Ubuntu 24.04.4 LTS.Yesterday I was able to flash my firmware to an module based on the STM32H755 MCU via ST-LINK using the following settings:Port: SWDMode: NormalReset mode: Soft...

BoardFront.png BoardBack.png

Resolved! snapdragon stlink interface

It seems like it's been over a year since reports surfaced that the ST-Link interface isn't working on Snapdragons.Are there still no ST-Link interface drivers available for Snapdragon CPUs?

changys by Associate
  • 839 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.