2022-10-17 1:37 AM
I am having an ELF file (created from a modm.io example) which gives a warning when loading it in the STM32CubeProgrammer tool. It mentions there are 'two or more segements that overlap', but the segments it lists in the log output don't overlap. :
segment[0]: address= 0x8000000, size= 0x1058
segment[1]: address= 0x10000000, size= 0x0
segment[2]: address= 0x20000000, size= 0x0Is this a bug in the tool or is there something wrong with my ELF file?
I attached the ELF file as reference.
2023-02-28 1:58 AM
I have the same problem.
Here as well : https://community.st.com/s/question/0D53W000020H1flSAC/elf-file-2-or-more-segments-define-the-same-memory-zone
I suppose that ELF files are not well supported.