STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

GDPR compliance of CubeIDE and CubeProgrammer?

I just downloaded and installed both STM32CubeIDE and STM32CubeProgrammer.They both forcibly installed with user-spying phone-home features how I use the software, while only mentioning how to disable the feature after they have been installed.So, th...

SOlen.1 by Associate II
  • 5998 Views
  • 10 replies
  • 4 kudos

The only routine folder in the \bin\ExternalLoader folder in the cubemxprogrammer2.18.0 installation folder is the stldr file

我使用 H750VBTx 芯片读取寄存器0x1FF1E7FE返回值如下所示参考 https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-2-18-0-released/td-p/747840 文章,我的芯片的 bootloader 版本是否无法使用 stm32cubeprogramme2.18.0 对外部 qspi 闪存进行编程?我在哪里可以获得 \bin\ExternalLoader 文件夹中的最新可用例...

keanlee0721_0-1740065135381.png

Resolved! Downgrade STM32CubeProgrammer in STM32CubeIDE

STM32CubeProgrammer v2.13 was giving me the famous "Failed to execute MI command" and "Failed to download Segment[0]" errors within the STM32CubeIDE, so I downloaded the standalone STM32CubeProgrammer v2.10 and it works fine. The IDE still uses v2.13...

CCend.2 by Associate III
  • 5771 Views
  • 7 replies
  • 3 kudos

Resolved! Change the location of Data_base folder

Hi all, I am working on my own program using the API provided with the stm32Cubeprogrammer V2.18 to flash custom bootlader and programs over USB in dfu mode. The problem I had was when I tried to flash a custom bootloader, the function connectDfuBoot...

Rafa096 by Associate II
  • 1508 Views
  • 2 replies
  • 1 kudos

Unable to detect the chip after programming

 I am programming my STM32F423RHT6. But due to some reason, suddenly I am unable to code the MCU. The connection is getting lost for some reason. I don't know what is the reason for this behavior.  I am attaching my code along with this message. The ...

Screenshot 2025-01-19 170709.png
vbk22398 by Senior
  • 14360 Views
  • 19 replies
  • 9 kudos