Solved
STM32Programmer V2.16.0 Missing BOOT bits in Option Bytes
Hello,
I will configure the boot mode in the option bytes of the STM32G030F6. Now I see only the nBOOT1. I missing the nBOOT_SEL and nBOOT0.

In the refernce manual are describe all:

How can I cinfigure it?
And after the programming I will reload the option bytes with setting of the OP_LAUNCH flag. Can I do it with the STM32Programmer and how?
Thanks for our help,
Bernd