STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Support for arm linux?

Hi. I have a request. Is it possible to compile STM32CubeProg for arm linux?Right now it is possible to compile firmware for stm32 on arm linux using the stm32duino toolchain from ST.However, the STM32CubeProg is only available on intel linux. This m...

koendv by Associate III
  • 10475 Views
  • 9 replies
  • 8 kudos

STM32 flash and reset from GPIO of Raspberry PI

Hello, I have managed to use stm32flash to flash custom binary to the STM32 through the raspberry pi.This involves moving BOOT0 to 0V, pressing reset and running the command.I can also include -R to software reset the STM32 after this is finished.I t...

TClar.1 by Associate
  • 2796 Views
  • 2 replies
  • 0 kudos

run STM32CubeProg on Raspberry pi 4

I don't see ARM 32/64 bit in the system requirements of STM32CubeProg. Is it possible to get this running on like a raspberry pi 4? I am interested in CLI onlyor do you have other suggestions on how i could do a flash of stm32 chip (STM32G070CB)

GHama.1 by Associate
  • 2394 Views
  • 3 replies
  • 1 kudos

Programming STM32F722RET6 from Raspberry Pi via UART

Hi,I would like to use a Raspberry Pi to program the STM32F722RET6 micro controller via the RPI UART. My Problem is, that the Cube Programmer is not made for ARM architecture, so it cant run on the Pi.I cant find a solution for this, apart from emula...

PLuca by Associate
  • 1712 Views
  • 2 replies
  • 1 kudos