STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! External Loader

Hello all,I have a custom board with an STM32U5A9 mcu with an external MT25QL128 flash for TouchGFX assets.I have a working loader for IAR Embedded workbench and I'm trying to port it to work with the STM32CubeProgrammer.When building as a normal pro...

RW3562 by Associate II
  • 2193 Views
  • 6 replies
  • 1 kudos

Making the DTR/RTS option support CH340

Almost all development boards produced by Chinese vendors use CH340 as the uart converter chip, I would like stm32cubeprogrammer to be able to control the RTS and DTR of this chip.If the feature works fine for the FT232RL, I don't know why it won't w...

wc7086 by Associate II
  • 7414 Views
  • 9 replies
  • 0 kudos

BLE test with the STM32U5 board

Hey, I'm just trying to use the BLE STM32UB5x in the board B-U585I-IOT02A. I used the following configurations for the STM32CubeProgrammer like suggested here (https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_Hardware_Setup)SW4 OFF, SW5 ON,...

Unable to update firmware

I want to use stm32H5 series microcontroller and I am trying to write from STlink... I can access the microcontroller by SWD (I can check Option Byte), but I can't write. I can write to the USART via the bootloader with TrustZone disabled, but... I w...

Satoshi1 by Associate II
  • 1183 Views
  • 4 replies
  • 0 kudos

External loader issue with STM32H743 and W25Q512

Hi all,I am working on the development of an external loader for STM32CubeProgrammer.CPU is STM32H743, flash memory is W25Q512 in quadspi mode.I have a problem in indirect mode: it's working (read and write), but in read I have long timeouts: //Send ...

lucky65 by Associate II
  • 867 Views
  • 3 replies
  • 0 kudos

Resolved! External loader issue with STM32H743 and W25Q256

Hi,I am using Clives loader for the STM32H with the correct pins etc but it never works in the STM IDE, so I thought I would follow controllertechs videos to try and make my own loader, that didn't work either, but I did verify all the QSPI parts rea...

mtechmatt_0-1725012574894.png
mtechmatt by Associate III
  • 6472 Views
  • 13 replies
  • 1 kudos