Skip to main content
Tajwar.Chandel
Associate III
June 19, 2023
Question

Error: No STM32 Target found! If your product embeds Debug Authentication,

  • June 19, 2023
  • 11 replies
  • 13912 views

Hi,

We are facing a issue to connect the ST link with our hardware setup ,,,, in today morning this is working fine but in afternoon facing the error in connection with the STlink debugger found error " Error: No STM32 Target found! If your product embeds Debug Authentication, please perform a discovery using debug Authentication." 

Target voltage showing :- 0 or sometimes 0.22v (after refreshing) 

TajwarChandel_0-1687180319452.png

Please suggest. 

This topic has been closed for replies.

11 replies

AScha.3
Super User
June 19, 2023

Hi,

0V from target: check voltage with dmm at your target, maybe it is really low.

You have any other target board, to check the st-link is working ok ?

 

If you feel a post has answered your question, please click on " Best Answer ".
Tajwar.Chandel
Associate III
June 20, 2023

Hello Ascha,

We have facing the same issue on 2 numbers of boards from yesterday afternoon.

Regards,

 

ST Technical Moderator
June 19, 2023

Hello @Tajwar.Chandel 

Try to switch to Power down Mode in ST Link Configuration.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Tajwar.Chandel
Associate III
June 20, 2023

hi,

not connected under power down mode as well.

 

Regards,

 

Tajwar.Chandel
Associate III
June 20, 2023

Hi @Belaid,

Tried many times but still failed to connect. 

AScha.3
Super User
June 20, 2023

>same issue on 2 numbers of boards from yesterday

so - you have many boards, and some working ok ?? or was it working before ?

If you feel a post has answered your question, please click on " Best Answer ".
Tajwar.Chandel
Associate III
June 20, 2023

Hi,

One more thing that this issue came after downgrade the firmware.

The MCU used STM32WB55RGV6.

Please suggest.

 

Regards,

Tajwar

Visitor II
December 21, 2023

same problem with two boards and no resolve problem?

 

Associate II
September 9, 2024

Is there still no solution? Got the same Board and the same Problem 

Tajwar.Chandel
Associate III
September 9, 2024

Hello,

No solution.