STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resetting target via reset pin

Hi! I'm trying to program a Creality 3D printer 4.2.5 board with an STLINK. This board has a STM32F103RE MCU. I've already successfully flashed this board more than once before with STM32CubeProgrammer. I recall at first it wasn't allowing me to conn...

JPFF by Associate II
  • 873 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer v2.20 released

We are pleased to announce that STM32CubeProgrammer 2.20 is available What is new in 2.20: • Support for the STM32MP21x microprocessors:         – External memory programming        – OTP programming        – PKCS#11        – ST power management IC• ...

Resolved! STM32Cube Programmer installation error

Hello, Stm32cubeprogrammer installation does not proceed to the final stage, it remains at step 8 and is not completed. I tried the program on three different PCs with administrator rights, the result is the same, the installation does not complete.

st32prog hata.png
Soner23 by Associate II
  • 15814 Views
  • 24 replies
  • 13 kudos

Program bin file from Cube Programmer

I have two stm32f429 Discovery boards. I programmed one of the board using cube ide; the output of which was as expected. Then using cube programmer I read and saved the bin file from that board. Using that bin file I programmed my another board whic...

MGogr.1 by Senior
  • 2004 Views
  • 8 replies
  • 1 kudos