STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Mass erase failing - STM32H533RET6

Hello,I have a custom STM32H533RET6 board that I can't program.  Following advice found on the ST website I am trying to use CubeProgrammer to mass erase the flash, however it is failing to do so.I am using an STLINK-V3MINIE with Mode: Under reset an...

Resolved! Cannot download STM32CubeCLT

I am logged into my STM user account.I get to the download page for STM32CubeCLT (https://www.st.com/en/development-tools/stm32cubeclt.html#get-software) and I try to download the latest version for Windows.A dialog pops up with 'Log in to MyST', 'Cr...

MWils.4 by Associate II
  • 5797 Views
  • 6 replies
  • 3 kudos

Resolved! Empty lines added by --safelib command into .hex

Starting from V2.13 the STM32CubeProgrammer_CLI adds strange empty lines into the .hex file when adding CRCs using the --safelib command.Example:...:20F9C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF47:20F9E000FFFFFFFFFFFFFFFFFF...

DFlam.1 by Associate
  • 995 Views
  • 2 replies
  • 0 kudos

Resolved! STM32N6 Flash Memory Protection

I'm trying to flash an an NUCLEO-N657X0-Q board with the STM32N6 using STM32CubeProgrammer v2.20.0. I have two NUCLEO-N657X0-Q boards here: One of them flashes just fine, the other one refuses to work. Both boards are in development mode (BOOT jumper...

Jeija_0-1761678820914.png
Jeija by Associate
  • 863 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer proper jlink error handling

It would be great if the STM32CubeProgrammer would do proper error handling for J-Link debug probes instead of crashing.Issue:Every times I try to the connect to a STM32 target that is not powered, or not properly connected the GUI pops up three erro...

Tom_pm by Associate III
  • 679 Views
  • 1 replies
  • 1 kudos