cancel
Showing results for 
Search instead for 
Did you mean: 

MCU isn't recognize

AndrewFFFF
Associate III

Hello to everyone

I'm working with NUCLEO-C071RB.

I debug , all OK.

Because now i want bliud my board i tried to connect with the software Programmer with my ST/link2 device (external)

I disconnected JP2-4-6-7 like shown in screenshot.

I power on the board with usb cable.

The Programmer seems recnognize the MCU (NUCLEO-C071RB), but so what does it means "target no found"?sdsfgd.pngddddd.png

 

regerttgterome.pngvfdfvfddfv.png

8 REPLIES 8
Andrew Neil
Super User

@AndrewFFFF wrote:

I power on the board with usb cable.

The Programmer seems recnognize the MCU (NUCLEO-C071RB), 


The on-board ST-Link is still connected to that USB - so the programmer will still see it.

But you have disconnected the target MCU from the on-board ST-Link - so it will say, "No target found"

 

Instead, you need to connect the programmer to your external ST-Link, and wire that ST-Link to the target MCU.

 


@AndrewFFFF wrote:

 my ST/link2 device (external)


Is it a genuine ST-Link ?

See: How to recognize a genuine ST-LINK/V2 versus a cloned one

In particular, anything looking like this is fake!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

 

Instead, you need to connect the programmer to your external ST-Link


Use this drop-down to select which ST-Link to use:

AndrewNeil_0-1743588763584.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Here  with the board power on.Senzanfdsome.png

Here after the run the software Programmer without power on the board.

zcxz.png

With both ST-Links connected to the PC, they should both be available in the drop-down list; eg,

AndrewNeil_0-1743594005306.png

You may need to press the 'refresh' button: AndrewNeil_1-1743594070193.png

 

Again, is your other ST-link a genuine ST one?

Please show (a) good, clear photograph(s) of your setup

 

PS:

You have to click the little arrow to get the list:

AndrewNeil_2-1743594276666.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
AndrewFFFF
Associate III

I connected only SWDIO, SWCLK, NRST,   VCC GND

so i can connect every jumpers, no conflit?

Those are the connections from the Target MCU to the ST-Link.

You also need to connect the ST-Link to the computer - via USB.

Again,  is your other ST-link a genuine ST one?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Here the photo

IMG_20250402_140104.jpg