STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! NUCLEO-N657X0-Q: Unable to erase flash

Hi,I've recently been trying to get an LRUN application up and running on the NUCLEO-N657X0-Q board. Similar to the posts in https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32n6570-dk-unable-to-erase-external-flash/td-p/757897, I cannot acces...

michaelg643_1-1755967138338.png michaelg643_0-1755966866504.png

STM32CubeProgrammer v2.21 released

We are pleased to announce that STM32CubeProgrammer 2.21 is available What is new in 2.21: • Support for the STM32WL3Rxx microcontrollers:         – Internal memory programming        – Option byte and OTP programming         – PKCS#11        – Firmw...

STM32CubeProgrammer erase fails under Linux

I noticed that the V 2.20 STM32CubeProgrammer erase function doesn't work under Pop_OS!, a Linux distribution.  It does however work on Windows 10.  I don't think this is a logic failure within the STM32CubeProgrammer but some weird interaction with ...

Resolved! Automate Production Programming

Hello Team,To address mass Programming of Customized board , Looking help to have Batch File / Python Script which accomplishes Following Task :1. Flash The Hex file2. Set RDP13. Read UID (96-bit ) of MCU4. Log UID and Time into CSVI tried with batch...

bsuthar by Senior
  • 1472 Views
  • 12 replies
  • 2 kudos

STM32G431 STProgrammer Writing Error

I am experiencing issues when attempting to upload the code to the MCU mentioned above on my board. I am trying to upload the code using the programmer on the STM32F407 Discovery board. It reads the chip, it erases the chip, but it does not upload th...

cereyanmhendisi_0-1763016190746.png

STM32CUBEprogrammer software bug

This software has too many bugs. Could the developers please look into the main issues? 1. If the downloader fails to connect, it spams dozens of error messages. 2. Frequent freezing, primarily when the downloader fails to connect—the software gets s...

zhaowhong by Associate III
  • 537 Views
  • 5 replies
  • 0 kudos