STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammers not starting on WIndows 10

Just like the title says: the STM32CubeProgrammers IDE V2.2 does not start on my pc. When I click to execute, I briefly see the program loading and then the splash screen disappears and nothing happens. No tasks running either in task manager. I also...

STM32CubeProgrammer 2.2.0 - Java issue

Hi there!I just installed the STM32CubeProgrammer and the GUI doesn't come up.O/S: (cat /etc/os-release )NAME="Linux Mint" VERSION="19.2 (Tina)" ID=linuxmint ID_LIKE=ubuntu PRETTY_NAME="Linux Mint 19.2" VERSION_ID="19.2" [...] VERSION_CODENAME=tina U...

Resolved! Oracle JRE license impact

https://www.freshconsulting.com/how-oracle-java-licensing-changes-affect/https://labs.consol.de/development/2019/02/05/oracle-license-is-the-free-lunch-over.html https://www.itassetmanagement.net/2019/02/21/oracle-java-new-licensing-model/ https://ww...

30 second timeout whilst programming external device with custom external loader in STM32CubeProgrammer

I have written an external loader for a device connected to my STM32F103 and I have debugged it and it works for the most part. Init(), Erase(), SectorErase(), Read() and Write() are all working ok, except when trying to program a large file. My exte...

Flashing one twin QSPI on the STM32H743I-eval

Hello,I'm not sure this problem could be addressed to the cube-programmer topic.I have a STM32H743I-eval and modified from the default two QSPI mode to the one twin QSPI.The external load doesn't work any longer after that whatever options I select.C...

Luke3 by Associate II
  • 2097 Views
  • 4 replies
  • 1 kudos