STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer STM32G474 option bytes / IWDG

Dear allIf we clear the IWDG option (enable watchdog by hardware at bootup), we cannot undo this.In that case we have to use the old STM32 ST-LINK Utility tool.STM32CubeProgrammer version: v2.11.0µC: STM32G474RBT3The problem seems to be PC dependent!...

FWege.1 by Associate III
  • 3187 Views
  • 3 replies
  • 0 kudos

Resolved! setVerbosityLevel of the API

I am calling setVerbosityLevel of the API with CUBEPROGRAMMER_VER_LEVEL_NONE (0) in the C++ USB Example project supplied but the DLL routines (like connectDfuBootloader) are still outputting messages. Still there any way to stop these messages?

STM32CubeProgrammer Issue erasing sectors past 127

Using STM32CubeProgrammer V2.11.0 on Windows 10I have issues erasing sectors past 127 on the STM32L496RET6 MCU.Erasing sectors 0-127 appears to work okay.Erasing sectors 128-255 does not show an error, however when I re-connect the programmer to the ...

Sde B.1 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

Did I brick my STM32F2?

Hi all -I'm modifying some legacy code written for a WICED device that contains an STM32F2xx. The original programmer had a passage that reduces down to:#define OB_RDP_Level_0 ((uint8_t)0xAA) #define OB_RDP_Level_1 ((uint8_t)0x55)   FLASH_OB_Unlo...

mzimmers by Associate II
  • 2095 Views
  • 2 replies
  • 0 kudos

Error: Download verification failed

hii am using STM32H745BIT6, i am using a st-link v2. i was able to debug until Friday but suddenly it stopped and gives me this error.STMicroelectronics ST-LINK GDB server. Version 7.0.0Copyright (c) 2022, STMicroelectronics. All rights reserved.Star...

fMoha.1 by Associate II
  • 1733 Views
  • 1 replies
  • 0 kudos