STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to use the program load header for the debug environment flash algorithm while using the STM32CubeIDE?

Hi there,it seems that STM32CubeProgrammer (Version 2.6.0) is using the program load header information to flash the system, while the STM32CubeIDE (Version 1.8.0) is using the section information. Since the initialize data section is not part of tha...

BMäme.1 by Associate II
  • 2935 Views
  • 8 replies
  • 0 kudos

Help to put stm32 32f042 in boot mode

Help to put stm32 32f042 in boot mode.I have this board from aliexpress and i want to load a project with STM32CubeProgrammerhttps://www.aliexpress.com/item/1005001417495721.html?spm=a2g0o.order_list.0.0.21ef18026yFGOLI receive this error and i think...

mm.4 by Associate II
  • 3544 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeProgrammer does not work with Windows 11.

I have the following problem. I recently installed Windows 11 and tried to install the STM32CubeProgrammer. But non of the following versions work with Windows 11STM32CubeProgrammer 2.11.0STM32CubeProgrammer 2.10.0STM32CubeProgrammer 2.9.0I always ge...

0693W00000Sv9rAQAR.png
TWolf.2 by Associate
  • 3510 Views
  • 2 replies
  • 0 kudos

MCU STM32F733ZE doesn't START

Hello Community,We have an issue on a design with an MCU STM32F733ZE on a custom electronic board, we don't manage to program it through STM32Cubre Programmer ("No STM32 found"). We observed that the power consumption is very low, less than 0.1mA so ...

SFELL.1 by Associate II
  • 4252 Views
  • 6 replies
  • 0 kudos