STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Version 2.13.0 on macOS memory leak?

when running STM32CubeProgrammer 2.13.0 under macOS 13.2.1 Ventura on Apple M1 the application allocates excessive amounts of Memory. This was observed when running the programmer in automatic mode for several days. The allocation was about 69 GB. M...

0693W00000aJdH8QAK.png
KaiS1 by Associate
  • 1397 Views
  • 1 replies
  • 1 kudos

Resolved! How to write bytes to flash without restart?

I am trying to use the windows version of STM32_Programmer_CLI.exe (version 2.13.0) to write bytes to a flash (windows 10). The command I am using is like./STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -w8 0x08080000 0x00 0x00 0x00 0x00 0x00 0x00...

ADiet.1 by Associate III
  • 6614 Views
  • 13 replies
  • 0 kudos

UART connection mode problems (2.13)

Platform: Windows 11 22H2 (x64)CubeProgrammer version: 2.13I've got 2 devices:HW Controller which uses dual FTDI drivers (2 COM ports; 1 port connected to ST microcontroller and 1 port connected to ESP32)HW Adapter which uses software virtual COM (ST...

Aelavin by Associate II
  • 1618 Views
  • 0 replies
  • 0 kudos

Resolved! Program flashed in reverse (MSB LSB)

Hello, I am using an STM32F427ZIT6 on a custom board for my project and it was working perfectly until now. I was able to programming it with an ST-Link V2 + ST-Link Utility as expected.I was working on adding DMA to my code but one day my chip stopp...

0693W00000aJfkbQAC.png 0693W00000aJfl5QAC.png 0693W00000aJfljQAC.png
PSicl.2 by Associate II
  • 3925 Views
  • 3 replies
  • 0 kudos

Resolved! STM32_Programmer_CLI.exe write file with space in path

Hi,I'm using STM32CubeProgrammer CLI (2.13.0).I'm trying to write a file to my device using this command :"C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -C port=SWD mode=UR -vb 1 -e all -w "%fir...

CThie.1 by Associate II
  • 8225 Views
  • 10 replies
  • 0 kudos

How to update the STM32CubeProgrammer?

On windows 10 I have version 2.12.0 installed of the STM32CubeProgrammer, but on command line I have version 2.13.0. In order to update the GUI version to 2.13.0 as well I use the "Help" -> "Software update" button but I see the following: so either ...

0693W00000aJYqSQAW.png
ADiet.1 by Associate III
  • 1302 Views
  • 0 replies
  • 0 kudos

Resolved! Bug in command line tool or GUI version?

I am using the GUI version and the command line tool to work with a device, but one of these tools has a bug. Checking which bank is use to boot from I get clearly contradictory results. See screenshot. Which tool tells me the bank used to boot from?...

ADiet.1 by Associate III
  • 3710 Views
  • 5 replies
  • 0 kudos

Resolved! How can I use the STM32CubeProgrammer windows executable to read a memory area without the device resetting?

I have been trying to read a memory area as follows on windows power shell:.\STM32_Programmer_CLI.exe -c port=SWD -r8 0x08080000 8 -r8 0x08080C00 8but that triggers a reset of the device. I do not want a device reset, I just want to read the memory a...

ADiet.1 by Associate III
  • 10494 Views
  • 23 replies
  • 1 kudos