STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Programmer not able to find target

Hello everyone,I'm using STM32CubeIDE 2.1.0 and STM32CubeProgrammer on Ubuntu 24.04.4 LTS.Yesterday I was able to flash my firmware to an module based on the STM32H755 MCU via ST-LINK using the following settings:Port: SWDMode: NormalReset mode: Soft...

BoardFront.png BoardBack.png

Resolved! snapdragon stlink interface

It seems like it's been over a year since reports surfaced that the ST-Link interface isn't working on Snapdragons.Are there still no ST-Link interface drivers available for Snapdragon CPUs?

changys by Associate
  • 736 Views
  • 5 replies
  • 2 kudos

Resolved! No ST-Link Detected

Hi,I'm having trouble getting my ST-Link V2 dongle to be recognized by Cube Programmer. It is recognized by Windows 10 in the device manager, I have been able to update the firmware, and I can get it to load in STM32 ST-Link Utility, but that program...

jrronzani_0-1766544405084.png jrronzani_1-1766544502317.png jrronzani_2-1766545099083.png