cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer upload fail after update to 2.20

heveskar
Senior

Basically continuation of https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-upload-fail-after-update-to-2-20/td-p/825113 - after fixing the hex to correctly span both the banks, upload error (using ST-Link) still persists. Firmware can be uploaded using USB bootloader, just the ST-LINK upload fails. It seems that this is a bug of the STM32CubeProgrammer.

STM32CubeProgrammer v2.20.0.

I attach the firmware hex. I also attach log from the programmer.

@PKola.1 @STOne-32 @Maryem 

 

1 ACCEPTED SOLUTION

Accepted Solutions
heveskar
Senior

In STM32CubeProgrammer v2.22.0 mentioned problem is not present anymore.

View solution in original post

5 REPLIES 5
Maryem
ST Employee

Hello @heveskar ,

 

I appreciate your input. I will review this further and provide an update shortly.

 

Thank you,

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TDK
Super User

Still doesn't make sense to me that it "worked correctly" in 2.19. How could it work correctly if the memory map was incorrect? Is flash physically present but 2.20 is doing more bounds checking than 2.19?

If you feel a post has answered your question, please click "Accept as Solution".

As per our reading of the forum, you are right, the memory is there, it is just not tested (link).

Maryem
ST Employee

Hello @heveskar,

 

Thank you for your patience. 

I confirm the issue from my side. I’ve submitted an internal ticket for further investigation by the team. I will keep you updated.

Internal ticket number: 215926 (This is an internal tracking number and is not accessible or usable by customers).

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
heveskar
Senior

In STM32CubeProgrammer v2.22.0 mentioned problem is not present anymore.