STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

post build path

need to add CRC to my binary. i.e. srec_catCan I add path to IDE to look for srec_cat, alternative what path are searched

Could not disable RDP at STM32WB55CEUX chip in my custom board

I had a problem while uploading firmware into my custom board.​I used ST-Link attached at NUCLEO-F091RC board, and I could read Option Bytes and Memory at 0x00000000 using ST-Link Utility and STM32CubeProgrammer.​​But I can't read or erase flash memo...

0690X00000ARNzmQAH.png 0690X00000ARNzwQAH.png 0690X00000ARO19QAH.png
qpdkvn by Associate
  • 10587 Views
  • 13 replies
  • 1 kudos

I need help setting the secure area on STM32H753 MCU

Hello,I need help setting the secure memory area for the STM32H753XI mcu. I am running it on STM32H753I-EVAL kit.I have read the dedicated part on the reference manual (chapter 5 on document RM0433), the "Introduction to STM32 microcontrollers securi...

LSans.1 by Associate
  • 2265 Views
  • 2 replies
  • 0 kudos

Resolved! RM0438 RNG htcr reg config && rng_cr

hi there I cannot figure out the true meaning of htcr reg and config1~config3 field in rng_cr reg。 I was wondering about the relationship between health test register and health test parameter (repetition counter test the “40�? consecutive bi...

Wxu.1 by Associate II
  • 2161 Views
  • 5 replies
  • 0 kudos

Resolved! Enabling PCROP with RDP level 0 causes board to crash

Hello,I have an unexpected behavior with a H753ZI board. After a very few steps, I ended up in a situation where PCROP seems to be enabled and RDP level is set to 0. For some reasons, this causes the board to freeze indefinitely, moreover after disco...

EBonv by Associate III
  • 3254 Views
  • 5 replies
  • 1 kudos

Resolved! Scripts unavailable SBSFU youtube video

In the video, "Security Part6 - STM32 security ecosystem - 02 Building the SBSFU" there are some scripts under the folder "STM32SecuWS" which are unavailable in the SBSFU download software. Where can I get these scripts? I am also struggling while fo...

APara.5 by Associate II
  • 2145 Views
  • 3 replies
  • 0 kudos

Question about STM32L562E-DK demo with "TFM application"?

Hi,I followed document "readme.txt" in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" to family with TFM, it work fine.My question:1: "press reset button or restart the board power" will lock the board. Please tell me what code in...

zqizh.1 by Associate III
  • 1168 Views
  • 2 replies
  • 0 kudos