Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6986 - Output voltage problem

Hello,I have a problem with the output voltage of 3.3VWith input power up to 6V everything is fine. But when I increase the voltage up to 24V, the output voltage slowly changes from 3,3V to 2,8V. The load is about 50mAI can't figure out what the prob...

schematic.png TOP.png 2.png 3.png

Resolved! measure motor load torque using the FOC Iq current?

I would like to measure motor load torque using the FOC Iq current. Am I correct that torque should equal Iq*Kt. I am using the ST Motor Control SDK 5.4. I have characterized the Kt of my motor. I calculate Iq [mA] = Iq_s16 * VDD [mV/(Rshunt*Gain*655...

jcysyk by Associate II
  • 2607 Views
  • 2 replies
  • 0 kudos

VIPER06 device marking

Please advise me where I can find the device marking for VIPER06HN. I was expecting to find it in the datasheet but it doesn't appear to be in there.What is the meaning for CHN on the top right side and for F04250 on the bottom right?Thank you.Paolo

20250109_160238.jpg
Paul79 by Associate
  • 1232 Views
  • 2 replies
  • 0 kudos

Power Backup by Super capacitor

    hi ,Aiming to have few minutes power  back up for  STM32 mcu with SD card incase main supply 5v goes OFF condition . Timer added for capacitor  charging time since initial current is will be little high .The above is setup enough ? or something s...

MMARI1_0-1736666737100.png MMARI1_5-1736666823233.png
MMARI.1 by Senior II
  • 1735 Views
  • 2 replies
  • 0 kudos

EVAL6498L Evaluation Board

Moved from Feedback forum.I am exploring the possibility of using the EVAL6498L Evaluation Board to reverse the polarity of a DC bias in my circuit, and I would like to confirm whether it suits my application.Application Details:Objective: To dynamic...

Resolved! VN9D5D20FN operating with Vcc 5v

Hello,We are looking to use VN9D5D20FN (SPI management and monitoring) as power distribution solution for our product. There are 4 channels which are fed from common output of a buck converter. The buck has 5V 3.2A max output and that goes into VN9D5...

Cio by Associate
  • 997 Views
  • 1 replies
  • 1 kudos

Resolved! What is the maximum error of STPM32?

Hello,in the Datasheet of the STPM32 the accuracy of the active power is 0,1% error over 500:1 dynamic range.Is this the best case error or the maximum error of the enerqy measurement after calibration?What does the dynamic range of 5000:1 mean?  

Stp1 by Associate
  • 1314 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.