Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPV1040 behaviour with a battery charger IC

Hello,I am wondering about the behaviour of the SPV1040 MPPT converter used with a battery charger (specifically the LTC4162-L but I think it would be similar with any battery charger IC). I need to charge a 2S Li-ion battery which is why I connected...

TBeno.1 by Associate
  • 1021 Views
  • 0 replies
  • 0 kudos

High frequency (high pitch beep) sound when start motor

Hi,I'm using STM32F303RB with ihm08m1 to drive a 36V BLDC motor. When I start motor, a high frequency sound (like a high pitch beep) is being made in the motor. The sound is a problem and very annoying, is there any way or solution to avoid this soun...

Alex Chen by Associate II
  • 4065 Views
  • 9 replies
  • 0 kudos

STC3117 system integration

Application note AN4870 (architecture overview) refers to "Charger IC" connected to microcontroller via I2C and to STC3117 via CD.Can you indicate a suitable Charger IC ? My project is a "true" capacity tester for single Li-Ion cell (18650). Do you ...

ALomb by Senior
  • 2020 Views
  • 3 replies
  • 0 kudos

Resolved! What are STSPIN233 OC trip time (tOCSD) and OT trip time (tTHSD)?

Hello,the overcurrent and over-temperature trip (deglitch) times are not given in the datasheet.My focus is mainly on the OC trip time, that's because I intend on adding series inductors to the motor phases to protect from motor windings short, thus ...

SBore.1 by Associate
  • 1772 Views
  • 4 replies
  • 0 kudos