Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

viper16

At 350V dc voltage, Viper16  output is toggle for 2 s to 0V.  What could be problem? ..... Output req 24V @ 250mA and Input 200V to 350V DC. 

keyur1 by Associate II
  • 1920 Views
  • 1 replies
  • 0 kudos

L6470 Motor Driver Kval Parameter

I'm using the AN4144 Application Note to program the parameters for the L6470 Motor Controller. It shows that the Kval correlates with the desired voltage, or the target current multiplied by the motors' resistance.but the only other reference to Iph...

rtaImage.png rtaImage.png rtaImage.png rtaImage.png
EEMGOpx by Associate
  • 1214 Views
  • 0 replies
  • 0 kudos

I have a question about the microstep using the L6480 driver

I use L6480 stepping motor control driver. and I use microstep function (resolution 1/128)There was a problem that the motor did not move in a certain section when the motor was driven 1 step at a time with the microstep.This picture below is the par...

EnenJ_0-1687487278082.png
EnenJ by Associate
  • 1055 Views
  • 0 replies
  • 0 kudos

Resolved! EVALKIT-ROBOT-1 / MODBUS RTU / QUESTION

Hello Community​I try to test the EVELKIT-ROBOT-1 using MODBUS RTU.​I did it it's factory setting.After I had connect all the cables, I powered up the EVALKIT.​Motor turned to its init position and stoped at some point. ​And Motor hold that position ...

Mhan.1 by Associate
  • 2883 Views
  • 3 replies
  • 0 kudos

POWERSTEP01

Hello all,Does anyone know how to read the markings on a POWERSTEP01 part? Trying to decipher the date and lot code on parts we are using. Appreciate the help!

BGS by Associate
  • 1200 Views
  • 1 replies
  • 0 kudos

VNI8200XP Spice Model

i searched about the  spice model of  VNI8200XP (CAD resources ) to simulate with LTspice site but i couldn´t find  it , so could you provide it.thanks in advance  . 

ik97 by Associate
  • 892 Views
  • 0 replies
  • 0 kudos

2N5551HR LCC-3 Package Pin Orientation

Looking at the 2N5551HR datasheet pages 7 - 9, it is misleading where pin 1 is located. If you look at the UB package on page 7, pin 1 seems to be on the opposite side to the ident and dot. Does this also mean the LCC-3 package is also wrong. Can ...

I'm using the STC4054 Li-ion single cell charger in a design, the CHRG pin is supposed to have a weak pull-down when not charging but the current drawn is higher than specs

In the STC4054 datasheet, it says the CHRG pin is supposed to have a weak pull-down of max 35uA when no battery is connected yet. However, with a 4.7Kohm pullup from that pin to 3.3v, I measure a 1.2v drop, which indicates about 250uA of current. Wit...

PVaca.1 by Associate
  • 1258 Views
  • 2 replies
  • 0 kudos