2022-11-29 3:44 AM
Hi all,
I am using a 4-wire fan supplied by 24V. I was wondering if the tacho output from the fan needs an external timer or a Freq to voltage converter; or can I just use a pull up resistor and connect the tacho signal straight to the input of STM32 using one of its internal Timer.
I appreciate your help!
Regards,
Sabrine
2022-11-29 6:43 AM
Hello @SHamm.2,
the first suggestion is to check the specifications of the tacho signal on the fan datasheet (output type, pulses per revolution).
If it is a open-drain (open-collector) output a pull-up resistor to supply motor voltage is needed. Then by adding a voltage divider you can get the appropriately shifted signal than can be connected to the STM32 GPIO.
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.