Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Devices marking

Hello, I have some doubt on part number L9942XP1TR. What the meaning for letter "RR" on top mark. Can you provide some parts mark information? Thanks Man  

Manman_0-1688538883149.png
Manman by Associate III
  • 2689 Views
  • 2 replies
  • 1 kudos

Parts marking

Hello,Is it normal for parts marking? Please find the attached photo.ThanksMan 

IMG_20230711_215608.jpg
Manman by Associate III
  • 1555 Views
  • 1 replies
  • 0 kudos

Can I use the STUSB4500BJR under these conditions?

Power is supplied by connecting the STUSB4500BJR to the TypeA connector of a personal computer via a TypeC-TypeA conversion cable. In this case, CC communication cannot be performed between the STUSB4500BJR and the PC. Can the STUSB4500BJR continue t...

ROJIKO by Associate
  • 798 Views
  • 0 replies
  • 0 kudos

Resolved! Power MUX or multiple power path controller ?

Hello,I am looking for a "power multiplexer", basically 2 or 3 MOSFETs as ORing diodes on one chip.TI has something like that (TPS2121), and although ST has a lot of power switches, MOSFETs etc in their portfolio, I don't find anything like that. (An...

LCE by Principal II
  • 2931 Views
  • 2 replies
  • 0 kudos

L6562A vs L6562AT

Comparing the datasheets, they appear to be the same. Is there a reason for the different part names?

Kimjunho by Associate II
  • 1552 Views
  • 1 replies
  • 0 kudos

STSPIN32F0/G4

Hi ST experts,Can STSPIN32F0 or STSTPIN32F4 to drive the SiC/GaN mosfet by the specification of Rdson = 73mOhm, 650V and 26A?Thanks.

STLearner by Associate III
  • 1718 Views
  • 2 replies
  • 1 kudos

What is the maximum current output of EVALMASTERGAN4?

Hi there, I would like to buy EVALMASTERGAN4 for testing GaN HEMT for my master thesis. (https://estore.st.com/en/products/evaluation-tools/solution-evaluation-tools/psu-and-converter-solution-eval-boards/evstdriveg600dg.html)Would you please let me ...

NK.5 by Associate
  • 1048 Views
  • 0 replies
  • 1 kudos

Hi, i have purchased an EVAL-L9963E-MCU and i am trying to test it with the STSW-L9963E GUI. I'am following the application note AN5696 but i am stucked at the third point of the connection section (see sreen).

The main issue is that when i enter 1 in the ID assignment, as i'm using the L9963, the ACK LED wont turn green but red instead. The D13 LED on the board behaves consistently with what is written in the application note i.e. is tuned on when the Conf...

0693W00000Sw0G2QAJ.png 0693W00000Sw0FdQAJ.png
SBas3 by Associate II
  • 6603 Views
  • 10 replies
  • 1 kudos

SPV1050 fails to start switching

Context: I have placed this part on a new design. I have a dev kit as well. A failure to start switching problem is duplicated on the dev kit that is setup in the default state (as sent by ST) for use in buck configuration, targeting a 4.2V float LiP...

Whitewater_1-1688130076227.png Whitewater_0-1688130016105.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.