STM32 MPUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Start Usb2 from u-boot?

hi, i'm stuck starting usbh_hs2 from u-booti can already start usbh_hs1 at boot, in order to load kernel and fs from an usb mass storage. i wish to do the same with usb_hs2, is that possible? is one configuration from DTS or from U-boot source code? ...

MBell.5 by Associate III
  • 397 Views
  • 3 replies
  • 1 kudos

Resolved! USB not found

I have problem to get USB to work. I'm using custom board but I know that USB works because if I boot the board with the delivered image (MyIR) the USB works. I'm using buildroot with the 5.10 kernel and the linux kernel configuration from bootlin gi...

jhi by Senior
  • 535 Views
  • 1 replies
  • 0 kudos

Resolved! USB compliance testing

Hi, and yet another question...We would like to perform electrical compliance testing on our USB ports. This requires each port to send a test pattern.Our board has one upstream and two downstream facing ports. The upstream port can be set into vario...

jvog.sen by Associate II
  • 799 Views
  • 2 replies
  • 0 kudos