Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wireless Charging solution Wiki

This Topic is used for Wireless Charging solution 1.Mcu C drive code: GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs 2. Python drive code, check attach file "Python_FT260_S...

willzhou_0-1717985741931.png
willzhou by ST Employee
  • 1841 Views
  • 13 replies
  • 5 kudos

STPM34 weird values reading his registers

Hi,I'm debugging a board with two STMP34 used to read voltage and current from L1 - L2 and L3 of a threephase system. The current signals comes from three different TA devices.The issue is: sometimes, reading a block of registers using the Metro_HAL_...

SteRogge_2-1726839139781.png SteRogge_1-1726838870158.png SteRogge_4-1726839712971.png SteRogge_3-1726839290450.png

WLC99Rx Stuck in DC Mode

I'm getting a STEVAL-WLC99RX and STEVAL-WBCTX70 configured for some testing and put the WLC99RX in DC mode (5V ono Vout). I cannot figure out how to get it back into Rx mode.It feels a little bit like a chicken and egg situation. I need to be in DC m...

Electrically Isolated Semiconductor Device - STGF15H60DF

I had previously asked in case # 00204067, if the subject part STGF15H60DF was UL approved for isolation and I was told that is was approved under UL catigory QQQX2.E81734 per the requirements of UL 1557. I was linked to UL File # E81734 with a highl...

Dart-Eng by Associate
  • 133 Views
  • 2 replies
  • 0 kudos

Wireless Charging solution Wiki

This Topic is used for Wireless Charging solution 1.Mcu C drive code: GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs 2. Python drive code, check attach file "Python_FT260_S...

willzhou_0-1717985741931.png
willzhou by ST Employee
  • 1841 Views
  • 13 replies
  • 5 kudos

GP244

Hi,This is a over voltage diode from a uC programmer that I blew. Can anyone tell me the value? Thank you for the help,Rob

L6235Q - Using DIR with PWM signal (DT0001)

I found an aplication (ST Design Tip - DT0001), that suggests a way of controlling motor speed, using a PWM signal on the DIR input.  Works fine for speed.  Note: we are not using a micro as shown in the DT90001. We are using our design.  And using P...

MikeSD by Associate
  • 268 Views
  • 1 replies
  • 0 kudos