Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB port testing - STCC5011 USB charging controller

Posted on July 24, 2015 at 20:54Hi,I'm interested in STMicroelectronics's STCC5011 USB charging controller. We are carrying out product testing for the Lighting Global program (http://www.lightingglobal.org/). As part of this testing, we will be tes...

garick by Associate
  • 716 Views
  • 2 replies
  • 0 kudos

L6470 Got(ABS_POS) doesn't start immediately

Posted on July 30, 2015 at 18:53I have had partial success in using the L6470 eval board.  However, I found that when I issue a GoTo (ABS_POS) command, it doesn't execute right away.  Interestingly enough, it starts executing after I send a ''disabl...

dvelasco by Associate II
  • 703 Views
  • 1 replies
  • 0 kudos

tech problem with L6470H disc board

Posted on July 24, 2015 at 02:56Hi, i get start to test a L6470H discovery board and got some problems:1.i try to connect board and pc with usb cable but it shows unknow device in windows device manager in win7-64bit but works fine in win xp 32bit.(...

L6470H disc board communication problem

Posted on July 24, 2015 at 04:17hii got a L6470H disc board and try to run the source code from (dSPIN_Firmware_Library_STM32) and (dSPIN Discovery Kit) project both of them get SPI communication fail: any read of spi get 0xFF, the board is new and ...

L6482 FILTER CAP

Posted on July 18, 2015 at 05:04What is the filter cap required for driving a stepper motor at 5 amps RMS? The schematic from ST shows 220uF 100V but no ESR data. I placed a United Chemi-Con 390uF 100V with an ESR of 28m ohms and a ripple current of...

rengholm by Associate II
  • 1264 Views
  • 2 replies
  • 0 kudos

L6474 -- much faster in forward direction than in reverse?

Posted on June 22, 2015 at 16:05I've been encountering a strange problem.  I can use the L6474 to move a stepper motor pretty fast in the forward direction.  When I flip the direction bit though, I find that I can't make it move anywhere near as fas...

dvelasco by Associate II
  • 997 Views
  • 2 replies
  • 0 kudos

Non-detected Stall L6482

Posted on June 30, 2015 at 15:58Running a bidirectional stepper at 30V with L6482 and getting actual stalls in 16-microstep mode -- under load the motor literally stops and hums, but nothing is reported back to software. It's like the driver has not...

akates by Associate
  • 710 Views
  • 1 replies
  • 0 kudos

stm32

Posted on June 10, 2015 at 10:16Can i interface a quadrature encoder to stm32 without using the channel 1,for example using the channel 2  and channel 3 .  

L6470 in HiZ state chip gets hot is it normal?

Posted on June 14, 2015 at 20:55Hello I am new to dSpin, but straight to the question.I have a L6470h setup on a protoboard using schematics found in the usermanual.But I see that the chip gets very hot even though it is in HiZ state. I measured the...

msciuka9 by Associate
  • 684 Views
  • 1 replies
  • 0 kudos