Skip to main content
Jon Enz
Associate III
February 16, 2024
Question

Flashing ELF with STM32CubeProgrammer Flashes Garbage Before Image

  • February 16, 2024
  • 6 replies
  • 3469 views

STM32CubeProgrammer v2.15

I'm having the same issue identified in the following post in the latest (as of now) version of STM32CubeProgrammer: https://community.st.com/t5/stm32cubeprogrammer-mcus/flashing-elf-with-stm32cubeprogrammer-flashes-garbage-before/td-p/154225

JonEnz_0-1708106714055.png

Can that discussion be re-opened or an update provided here?

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
February 16, 2024

I don't think it's actually closed to new input, but probably helps to start a new thread

@Houda GHABRI  @Nawres GHARBI  @STOne-32 

Not actually garbage, but .ELF header data, not sure if it keys on extension, case, or magic patterns..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jon Enz
Jon EnzAuthor
Associate III
February 17, 2024

It was marked as solved so I just wanted to make sure there was an "open" thread.

Pavel A.
February 17, 2024

@Jon Enz Which toolchain produced your .elf file?

Pavel A.
February 16, 2024

 [removed]

Aziz BRIGUI
ST Technical Moderator
February 20, 2024

Hello @Jon Enz ,  

 

For now, I can't reproduce the issue you're seeing with .elf files generated by CubeIDE or EWARM. When relocating an application for an STM32L476 for example, there is a segment in the beginning of the flash, however, this segment has nothing to do with .ELF overhead. I suspect it has to do with jumping to the main application, since removing it will prevent the relocated app from running properly.

As for this thread : https://community.st.com/t5/stm32cubeprogrammer-mcus/flashing-elf-with-stm32cubeprogrammer-flashes-garbage-before/td-p/154225. What I noticed when opening the attachment by @Rami Rosenbaum(using multiple elf parsers/viewers) is that the elf extension overhead is indeed pointed to by a load type segment in the program/segment headers.

AzizBRIGUI_0-1708431133089.png

 

That's the part interpreted by CubeProgrammer (and several other tools), and usually that's not the case in elf files, here's an example elf compiled with EWARM (with a relocated app).

AzizBRIGUI_1-1708431275398.png

So as stated by @Pavel A. & @Tesla DeLorean ,we need to know the toolchain you're using in order to investigate further. Attaching the .ELF file could also be helpful.

 

Thanks in advance,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Jon Enz
Jon EnzAuthor
Associate III
February 21, 2024

The toolchain used to generate the file was ARM GNU 10-2020-q4-major. I can confirm that loading the .hex file shows the data starting at the correct location.

Unfortunately I cannot share the project files directly, but I was able to create a reduced project that produces the same result. The .elf and .hex files are in the build directory of the attached file. You can re-run the build using the following commands.

Configure:

cmake -B build -DCMAKE_TOOLCHAIN_FILE=toolchain-embedded-arm.cmake -G "MinGW Makefiles" -DCMAKE_BUILD_TYPE:STRING=Debug

Build:

cmake --build build --target ELF-TEST.elf