STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Can't download the program!! :(

Hello, I want to download the program, STM32CubeProgrammer.Before log in, download tap was visible and connectable.However, After log in, download tap continues to load...I've been waiting a long time, but it doesn't stop!!! :(I also cleaned my cache...

imege.PNG
inkong by Associate II
  • 4029 Views
  • 4 replies
  • 3 kudos

please improve STMProg

Please Never use a popup any where in the app its extremely annoying, use a window I propse you call it "Console" or "LOG " .. oh what do you know you already have one!!!.. so please stop with the popups... also remove the Refresh button Let Connect ...

NCD by Associate II
  • 5209 Views
  • 10 replies
  • 0 kudos

Using st link v3 to program over CAN

Good day,I am attempting to program an STM32L5 MCU using an ST Link V3 over FDCAN. I am aware that on the breakout board for the ST Link V3 there is connector CN5 which has CAN RX and TX. On the microcontroller I have a CAN transceiver installed on p...

Eben_0-1717506462665.png
Eben by Associate II
  • 3432 Views
  • 5 replies
  • 1 kudos

Resolved! Can't download STM32CubeProg

On Ubuntu 24.04 I tried downloading the latest version of CubeProg using Firefox and Chrome (both updated to latest release).  I also tried downloading older version to see if those links work.  All downloads lead back to the tool's home page.  So fa...

Resolved! Use STM CubeProgrammer with Jlink?

Hi,during development I work with the CubeIDE and use JLink, it connects to the SWD-port of my STM-board properly and works like a charm within the IDE.Now we're about to program loads of different boards. From my understanding this is where the Cube...

BSchm.6 by Associate III
  • 9057 Views
  • 3 replies
  • 2 kudos