STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.16.0 released

STM32CubeProgrammer v2.16.0 release informationNew features:• Added the support for the STM32U0 series– Flash memory/option byte/OTP programming via the debug and bootloader interfaces– RDP regression with password• Added the support for the STM32H7R...

Resolved! DFU Firmware lost

Hi,My MCU is STM32F746ZG. When I want to use DFU to upgrade my board by STM32CubeProgrammer, It show "No DFU detected" in the port list. And I use "zadig" to try install DUF driver, it cannot find any STM DUF device, too.Do my DFU firmware lost in my...

cloud_liu by Associate II
  • 2667 Views
  • 4 replies
  • 0 kudos

STM32F103C8T6 no USB Detection

Hello,I designed a PCB with an STM32F103C8T6, and I've included the schematic below. I want to program it via USB, so I used designs I found online for the layout. The crystal is 16MHz. When I connect the USB to the computer, it detects a USB connect...

JTAPIE_0-1730897005656.png
JTAPIE by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer does not run on Fedora 41

Hello,I have installed a fresh STM32CubeProgrammer on my Fedora 41 Linux system, but I am unable to run it.After installation, I have tried running it both using the desktop menu entry and from terminal, however it never starts and crashes with the m...