STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM flashing tool via SPI

Hi,I am working on STM32G491KCU6 board.We are connecting STM to a linux based SoC via SPI. What we required is, we need to flash STM from SoC. We found stmflash binary which supports only through i2c and UART. Is there any tool that support flashing ...

Resolved! Can't connect to ST-Link with CLI

Hi there,I have an ST-Link V2 which i want to use for programming a .bin file to an stm32G0 MCU. Afterwards i want to set the RTC register to the time beeing. It already works "manually" but i wanted to write a script to automate the process.I alread...

vs_rzb by Associate II
  • 2174 Views
  • 3 replies
  • 1 kudos

Resolved! No STM32 target found - STM32G030K6T6

Hi, I'm making a board for UART and I2C communication.Please refer to the schematic below;  I put 5V External power supply at VBUS,and connects SWDIO, SWCLK, NRST, 3V3, GND to the STLINK V3 Minie. However it shows "No STM32 target found" message on S...

SungjaeKim_0-1737011644144.png