STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer cant use UART in Version 2.19.0

Hello,I am using the UART-Connection to programm an ST32G431.With SW 2.5.0 all is fine:13:10:11 : STM32CubeProgrammer API v2.5.013:10:25 : Serial Port COM4 is successfully opened.13:10:25 : Port configuration: parity = even, baudrate = 115200, data-b...

FN by Associate
  • 2979 Views
  • 1 replies
  • 1 kudos

Resolved! ST-LINK V2 (stm8 & stm32) Cannot connect

Hello!So i would like to ask for a little help. The STM32 is kinda new for me, i always did stuff on Arduinos. So i have a LoraWan E5 wich i want to program with ST-Link V2, but as soon as i want to connect to it (to the st-link) in the STM32CubeProg...