cancel
Showing results for 
Search instead for 
Did you mean: 

Use STM CubeProgrammer with Jlink?

BSchm.6
Associate III

Hi,

during development I work with the CubeIDE and use JLink, it connects to the SWD-port of my STM-board properly and works like a charm within the IDE.

Now we're about to program loads of different boards. From my understanding this is where the CubeProgrammer shoukd be used. But when starting it, the JLink is not recognised, it only tells me about some ST-Link which could not be found (which is correct as it does not exist).

So how/where do I have to configure the CubeProgrammer to work with the JLink?

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

Unlike CubeIDE, the CubeProgrammer  does not work with J-Link. But you can use the Segger J-Flash software for the same price.

View solution in original post

3 REPLIES 3
Pavel A.
Super User

Unlike CubeIDE, the CubeProgrammer  does not work with J-Link. But you can use the Segger J-Flash software for the same price.

Tom_pm
Associate III

Since CubeProgrammer 2.16.0 it is supported, you may update the answer.

 

See also other post .

I just connected to a target using CubeMXProgrammer v2.17.0 connected via a J-Link.