The FDCAN module generates timestamps for sent and received messages, and you can configure it to use TIM3 as the source. Unfortunately, the documentation is rather thin, so I am left with a few questions:Do TIM3 and FDCAN need to run from the same c...
For every single programming action, I seenot one,not two,not three,but at least 4 stupid message dialog boxes I needto click awayevery single one for every programmingaction.How do I disable this?
It is a flash block, so you should reprogram all option bytes after the erase. The reset is necessary to update the flash registers, and for the new settings to be used. If you only want the user byte for storage, this is not needed.Remember that the...
You want your high speed clock stopped when in Standby. What are you using to wake up again?Keeping PLLs running at 200 MHz output can cost you a few mA, but 7mA is pretty high and sounds like you have a couple peripherals still running from your hig...