STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32 Bootloader stuck in loop

Hello,I am trying to use the built-in UART bootloader on an STM32H7. I have two boards: one on which the bootloader works, and one on which it cannot connect.The board on which I cannot use the bootloader reports the following error when I try to con...

0690X00000AQmFVQA1.png
ST User by Associate III
  • 912 Views
  • 0 replies
  • 0 kudos

How to compile API with QT

Hello, I have tried to compile the API examples of the STM32CubeProg with Qt but as one of the DLLs is 64 bits, it fails to run. Is there any compiled version of the DLL for 32 bits?Regards,

luisf by Associate II
  • 1514 Views
  • 3 replies
  • 0 kudos

No Software Reset when I download .hex file in STM32L4 using STM32CubeProgrammer interface and ST-LINK/v2 programmer?

I am using STM32L4 in my project. To download my .hex into flash memory, I am using ST-LInk V2 programmer and STM32Cube programmer. I am successfully in loading my .hex file to STM32L4 using STM32Cube programmer, but I do not think STM32Cube programm...

Resolved! Error programming option bytes on STM32F7.

I'm trying to program the F7 option bytes via the UART bootloader using the command-line or GUI programmer and get an error. Other commands work fine. Here is the output:14:00:24 : STM32CubeProgrammer API v2.0.014:00:36 : Serial Port COM9 is successf...

rammit by Senior
  • 1973 Views
  • 1 replies
  • 0 kudos

Failed to erase memory (STM32F746G)

I am trying to upload a program to the board but i keep getting this errorError: failed to erase memoryRead/Write protection is disabled and firmware is up to date (V2J33M25) This is what i get in the LOG13:49:39:117 : Memory Programming ...13:49:39:...

khaaal by Associate II
  • 1412 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F103RB Nucleo board issue

I have an STM32F103RB Nucleo board.I'm trying to build a very easy LED example (see details section).I expect that both LEDs (one on the bread board, one on the nucleo board) are blinking every 500 ms. But only the one on the board is working.The str...

TSchr by Associate
  • 2660 Views
  • 2 replies
  • 0 kudos