cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103RB Nucleo board issue

TSchr
Associate

I have an STM32F103RB Nucleo board.

I'm trying to build a very easy LED example (see details section).

I expect that both LEDs (one on the bread board, one on the nucleo board) are blinking every 500 ms. But only the one on the board is working.

The structure can be seen on attached figures. On a bread board I have an LED (yellow -> 2 V) and a resistance (100 ohm) in series connection. To the nucleo board there are 3 cables:

- red: ground to + on bread board

- black: 3.3V to - on bread board

- white: D2 to resistance

I hope somebody can help me. Do you need any other information?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TSchr
Associate

I found the problem. One of the cables was broken.

But thanks.

View solution in original post

2 REPLIES 2
waclawek.jan
Super User

Is the LED connected with proper polarity? Try to turn it around.

JW

TSchr
Associate

I found the problem. One of the cables was broken.

But thanks.