STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

stm32cubeprogrammer no st-link detected amd win7

The ST-LINK / V2 programmer is not detected on my PCs.Before that, when I had a win7 x64 PC with a core i5 processor - STM32CubeProgrammer worked. I currently have a Ryzen 3600 win7 x64. I have installed the latest STM32CubeProgrammer 2.9.0 and am ge...

0693W00000HowfAQAR.png 0693W00000Howf5QAB.png 0693W00000Howf0QAB.png 0693W00000HowevQAB.png

Resolved! NUCLEO-G031K8 Reset not working?

HiI know that this is probably a brain fart on my side, but I am currently playing around with the NUCLEO-G031K8 and cannot seem to put the MCU into reset using the reset button on the Nucleo board. In fact, I am running a simple GPIO LED toggle prog...

0693W00000Hp4wOQAR.png
AAnth.1 by Senior
  • 1935 Views
  • 2 replies
  • 0 kudos

Resolved! We have a problem downloading to the STM32L100 processor. It was programmed using STLink. Now we want to use STM32CubeProgrammer. Writing is not possible! It is not possible to change the RDP value either. If we use STLink, all is OK.

 10:55:25 : ST-LINK SN : 0034003E3137510339383538 10:55:25 : ST-LINK FW : V3J8M3B5S1 10:55:25 : Board    : STLINK-V3MODS 10:55:25 : Voltage   : 3.29V 10:55:25 : SWD freq  : 8000 KHz 10:55:25 : Connect mode: Under Reset 10:55:25 : Reset mode : Softwar...

Entony by Associate II
  • 1656 Views
  • 2 replies
  • 0 kudos

Resolved! Why the chip STM32F446RCT6 flash size is 512KB, not 256KB?

I buy some chips marked STM32F446RCT6 which flash size should be 256KB.But when I connect it use STLINK, I found the real flash size is 512KB.I have save some data after the address 256KB successfully. And I can read out these data.Am I buy fake chip...

0693W00000HogzUQAR.png
llm by Associate III
  • 1886 Views
  • 2 replies
  • 0 kudos