Hi there,it seems that STM32CubeProgrammer (Version 2.6.0) is using the program load header information to flash the system, while the STM32CubeIDE (Version 1.8.0) is using the section information. Since the initialize data section is not part of tha...