STM32 MPUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error while compiling custom machine

Hi, I am trying to compile an OpenSTLinux image for a target "DK2_A7" custom machine.I've followed this guide and everything seems ok until 98% of the process when the following error occurs:ERROR: tf-a-stm32mp-2.4.r1-r0 do_compile: oe_runmake failed...

RBruè.1 by Associate II
  • 485 Views
  • 3 replies
  • 0 kudos

Resolved! Dongles for STM32MP157F

Hi everyone,I'm not sure if the following questions depends on OpenSTLinux - drivers for example - or STM32MP1 hardware.I have the STM32MP157F MPU and I would like to integrate Bluetooth 5.0 . My main idea was to connect a Bluetooth 5.0 dongle into m...

OBaselga by Associate III
  • 1037 Views
  • 3 replies
  • 0 kudos

LBEE5KL1DX-883 issue with SDMMC3

Hi.. thereHope all are doing well We have designed our own custom board by taking the reference of the DK2 board, in which we're using the LBEE5KL1DX-883 WiFi/BT module from Murata at SDMMC3 somehow, the module is unable to detect!after dmesg of the...

Resolved! STM32MP157AA3 LTDC

Hi all,I am currently using VisionSoM board : STM32MP157AAB3 board.I am trying to drive an LVDS display via a RGB to LVDS converter. Here is the datasheet link for it.The panel settings are as follows : panel { u-boot,dm-pre-reloc; ...

NPal.2 by Senior
  • 446 Views
  • 2 replies
  • 0 kudos