STM32 MPUs Embedded software and solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157-EV kit with led blink

Hello, I have dual core STM32MP157F-EV evaluation kit. I can connect via ST-link and install an application (This is installing on M4). And when I press the reset button, the application is deleted because the M4 core is RAM. I want it to work again ...

ABayl.2 by Associate II
  • 1091 Views
  • 6 replies
  • 1 kudos

PWM - output during Suspend mode

HiWe are using SEEED studio 102110318 module which uses STM32MP157CAC3 processor. We want to know if there is any way we can keep processor pin PD13 pin to low state in suspend state. We want the pin to maintain low state while in sleep mode. We have...

Srini by Associate II
  • 1005 Views
  • 4 replies
  • 0 kudos

Resolved! Boot UBIFS from dataflash (nor0)

Hi Everybody,I would like to completely boot kernel 5.10-dunfell (last year) from a 64MB dataflash (nor0). No mmc0 or nand0. Compiled the correct DTS with TF-A, U-Boot and kernel, I would like to use the following TSV for STM32CubeProgrammer:#Opt ...

ATringali by Associate II
  • 1563 Views
  • 5 replies
  • 0 kudos

Using Jtag/SWD in Linux

Custom PCB, STM32MP157C chip. Linux 5.7.10. Buildroot build. No issues - Linux boots to console prompt without trouble, no errors. I can view device registers and all memory regions using Segger Jlink via SWD in both SPL and UBoot. Once Linux starts ...

info by Associate II
  • 1046 Views
  • 1 replies
  • 0 kudos

Resolved! Command “ alsamixer�? doesn't work in SDK "en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15"

root@stm32mp1:~# uname -a Linux stm32mp1 5.15.24 #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 armv7l armv7l armv7l GNU/Linux root@stm32mp1:~# pacmd list-sinks-inputs No PulseAudio daemon running, or not running as session daemon. root@stm32mp1:~# alsa...

mteaching by Associate III
  • 2723 Views
  • 2 replies
  • 0 kudos